VW3A9908
ready assembled IP54 base plate - for ATV61 - to increase cable connections
Main

Hide
accessory / separate part category Connection accessories  
accessory / separate part type Plate  
accessory / separate part designation Ready assembled IP54 base plate  
product compatibility ATV61WD90N4  
accessory / separate part destination Increase the number of cable connections  
range compatibility Altivar 61  
 
Complementary

Hide
electrical connection 1 cable gland metal ISO50 for the motor cable
1 cable gland plastic ISO12 for the control cable or options
1 cable gland plastic ISO20 for the control cable or options
1 cable gland special plastic ISO32 for the network cable
2 cable glands plastic ISO63 for the control cable or options
4 cable glands plastic ISO16 for the control cable or options